Thermostats

Wireless FocusPRO Comfort System 5-1-1/5-2 Day Programmable Thermostat

Wireless and connected to convenience, ease and comfort

Here’s comforting news. With this thermostat, there are no wires, and cutting into walls isn’t necessary. It’s wireless, meaning you can place it anywhere in the home. There are also smart features such as monitoring and controlling your system with your smartphone, tablet or computer. For example, you notice your bedroom is warmer than you’d like. With Portable Comfort Control, you can check the temperature and lower it a couple of degrees without ever leaving the bedroom. The more you learn about this thermostat, the more you’ll like.

  • 5-1-1 Day Programming (one program for weekdays; separate program for weekends or Saturday/Sunday)
  • Simple to program
  • Large backlit digital display (also available in smaller standard screen size)
  • Displays outdoor temperature (with Wireless Outdoor Air Sensor)
  • Easy-access battery replacement
  • Built-in instructions
  • Five-year warranty
  • Professional installation
Wireless
Place anywhere in the home. No running wires or cutting into the walls. Requires RedLINK™ enabled Equipment Interface Module for wireless functions
Internet Connection
Enables you to monitor and control your heating/cooling system from a PC, smartphone or tablet (requires Total Connect Comfort Services)
Portable Comfort Control
Check and control temperature from anywhere in the home (with Portable Comfort Control)
Specs
  • Model numbers: YTH6320R1001, TH6320R1004, YTH6320R1114, YTH6320R1122
  • Kits include thermostat, Equipment Interface Module, and sensors
  • Thermostat dimensions: 3 9/16 in. High X 5 13/16 in. Wide X 1 1/2 in. Deep

Wireless-FocusPRO-Comfort-System

Focus-Pro-Gallery-912x528-1
Focus Pro FrontView
Focus-Pro-Gallery-912x528-2
Focus Pro FrontView
Focus-Pro-Gallery-912x528-3
Focus Pro FrontView
Focus-Pro-Gallery-912x528-4
Focus Pro FrontView

SUPPORT ARTICLES

Each Honeywell thermostat model has a unique number that can help you get support for your product faster and easier . Depending on your model, this number is preceded by the letters TH, T, RTH, CT, TL or RLV.

Please watch this video for a quick visual guide on how to find your thermostat model number:


The fastest way to see your thermostat model number is to look for it on your thermostat ID card. If you do not have a product ID card, the fastest way to find the model number is by removing the thermostat from the wall-plate. Depending on your model, the thermostat will separate from the wall-plate with moderate pressure or there might be small screws holding the device in place. After removing the thermostat, flip it over and look for the model number, which is printed on the back of the case, starting with the group of letters mentioned above.

If the thermostat is battery operated and the batteries are accessed from the front of the thermostat, please check the area around the batteries. You can also check this list of our battery operated thermostats to find your model number.

If your thermostat has a mechanical clock, the model number is on a sticker on the horizontal surface above the clock.

The FAN selection key has two or three positions: Auto and On and sometimes Circ (Circulate). The Auto position will allow the system fan to operate whenever the heating or cooling system is turned on by the thermostat. The On position will turn the fan on to run continuously, regardless whether heating or cooling system is turned on by the thermostat or not. The Circ (Circulate) position if available will run the fan approximately 35% of the time, minus any time the fan will run with the heating or cooling system.
Honeywell offers thermostats for both low voltage (24 volts) and line voltage (120 or 240 volts) systems. The most common type of voltage from a central heating and/or cooling system is 24 volts (24Vac). The old thermostat may say somewhere on the thermostat that it is for 24 volt (24Vac) or maximum 30 volts (30Vac). If you see 120 Vac or 240 Vac on the thermostat, a low voltage thermostat will NOT work with your system. You will need a line voltage thermostat. This type of voltage is common with electric baseboard heating. Regardless of the voltage, Honeywell strongly suggests that you turn off the power to the system at the furnace, at the fuse, or at the circuit breaker panel before installing or replacing a thermostat. If you are unsure about your voltage, please contact a local heating and cooling contractor in your area for assistance.
Yes, the packaging contained with the thermostat is recyclable. Information about recycling thermostats containing mercury can be found at: thermostat-recycle.org/
Your thermostat is designed to control temperature to +/- 1 F. How often your heat turns on and off depends on several factors including the type of heating system you have and load conditions (in other words, how hot or cold it is outside). A typical mid-efficiency forced air system will cycle about five times in an hour (5CPH) under typical load conditions. A typical high efficiency furnace or hot water system would cycle less than that. The installer can adjust the cycle rate setting on the thermostat.
The thermostat takes the temperature override as a need to reach the new temperature setting right away. It will run the second or third stage only as long as necessary to reach new temperature setting.
"Auto" under "System" indicates that it is setup to automatically switch between heating and cooling. If your thermostat does not show auto, you may not have this feature.
The changeover valve is a device which reverses the flow of refrigerant in the heat pump. This will allow the freon to reverse and heat the home or cool the home. Honeywell uses an O terminal to energize the valve in cooling and a B terminal to energize the valve in heating. Some manufacturers of heat pumps may use the B terminal to energize in heating, while a vast majority energize the O terminal in cooling.
A heat pump uses the outdoor unit for both heating and cooling. Often the heat pump also has some sort of backup or auxiliary heat for when it is cold outside. The backup or auxiliary heat could be electric heat strips or a fossil fuel furnace. Thermostats that control heat pumps with backup or auxiliary heat typically have an Em Heat (Emergency heat) position. When the system switch is moved to the Em Ht. position, the auxiliary heat is activated on a call for heat. The compressor is disabled. If replacing a thermostat on a heat pump system, verify your thermostat is compatible.
Honeywell thermostats do not have the capability of making an audible noise such as a beeping sound. The noise you are hearing is likely from another electronic device which is near the thermostat. Check for a smoke detector, door bell, or security system.
Honeywell digital thermostats are designed to display the room temperature in a way similar to how people sense temperature. This means the thermostat takes into account not just the ambient air temperature but also the radiant temperature of objects in the room (i.e., wall and furniture). Room thermometers often only read ambient air temperature so they will not match the thermostat reading. Also, Honeywell thermostats do round in the display to the nearest whole number (half number in Celsius) and to the temperature setting. For example, if you have the thermostat set to 72 degrees the system will turn on and off but the inside reading on the thermostat never changes from 72. The actual temperature did fall to 71 or up to 73 and that is what turned on the heating or cooling but the thermostat display will stay at 72 to avoid jumping up and down constantly.
There are several items you can check. First check that the thermostat is set to the Cool position. Make sure the temperature is set lower than the Inside temperature reading. Also check the circuit breaker and reset if necessary. Make sure that the furnace door is closed securely. If “wait” is in the screen or “cool on” is flashing – wait 5 minutes for the system to safely respond. The thermostat will indicate it is asking for the cooling to turn on when "cool on" or a "snowflake" in the display. If this message is in the display, the thermostat is asking for the heat to be on and there is a likely a problem outside of the thermostat preventing the cooling from running.
There are several items you can check.
  • First check that the thermostat is set to the Heat position. Make sure the temperature is set higher than the Inside temperature reading.
  • Also check the circuit breaker and reset if necessary.
  • Make sure that the furnace door is closed securely.
  • If “wait” is in the screen or “heat on” is flashing – wait 5 minutes for the system to safely respond.
  • The thermostat will indicate it is asking for the heat to turn on when "heat on" or a "flame" in the display. If this message is in the display, the thermostat is asking for the heat to be on and there is a likely a problem outside of the thermostat preventing the heat from running.
Please see the steps below to troubleshoot this issue:
  1. Verify the call for heat is being made
  2. Check the configuration of the thermostat to make sure it is controlling the equipment properly.
  3. Verify that the thermostat is wired correctly.
  4. Make sure all of the wires are secure and in the correct terminals.
  5. Make sure the voltages are between 18 and 30 VAC or 20 and 30 VAC depending on the thermostat model.
  6. Make sure the thermostat faceplate is firmly in place against the wall plate

For more information on the Honeywell heating and cooling systems, please click here to see a list of instructional videos.

The thermostat has a feature called Adaptive Intelligent Recovery(AIR) or Smart Response or Early Start. This allows the thermostat to "learn" how long the heating and cooling system will take to reach the programmed temperature settings. So the temperature is reached at the time you set. For example: Set the Wake time to 6am, and the temperature to 70F. The heat will come on before 6am, so the temperature is 70F by the time you wake at 6am. The message "recovery" is displayed when the system is activated before a scheduled time period.

For more information, please watch this instructional video:

If we weren't able to answer your question please visit Help & Support

Need support for this product?