Thermostats

Prestige IAQ

Comfort has a prestige address

Our Prestige® IAQ has the features to make life at home easier, more inviting and ever so comfortable. For example, the color display can be easily read, and it can be changed to match your home’s décor. Programming is simple and easy, too. The system interviews you and uses the answers to your questions to program itself. You also can connect to the Internet to bring thermostat control to your smartphone, PC or tablet. Review and change the temperature in your home anytime and anywhere.

  • Seven-day programming
  • Displays outdoor temperature (with Wireless Outdoor Air Sensor)
  • Trilingual (displays in English, Spanish or French)
  • Five-year Warranty
  • Professional installation
High-Definition, Full-Color Display
It’s visually stunning and easy to read
Interview-Based Programming
The system interviews you and uses your answers to program itself. No need to work through complicated settings and instructions.
Internet Connection
Enables you to monitor and control your heating/cooling system from a computer, smartphone or tablet with the Total Connect Comfort app
Portable Comfort Control
Control or check temperature from anywhere in the home by using the remote
Time-of-Use Scheduling
Automatically adjusts your home’s temperature based on utility pricing to help save you money on energy costs
Specs
  • Model numbers: THX9421R5021WW
  • Color: White
  • Dimensions: 3-1/2 in. High, 4-1/2 in. Wide, 7/8 in. Deep

SUPPORT ARTICLES

No. Each thermostat can only be controlled by one Portable Comfort Center. But you can connect up to 16 different thermostats to one Portable Comfort Center to easily control multiple zones.

Yes. When connected with an Outdoor Sensor, select thermostats and devices will display the outdoor temperature and humidity on the screen.
The thermostat has a feature called Adaptive Intelligent Recovery(AIR) or Smart Response or Early Start. This allows the thermostat to "learn" how long the heating and cooling system will take to reach the programmed temperature settings. So the temperature is reached at the time you set.
There are several items you can check. First check that the thermostat is set to the Cool position. Make sure the temperature is set lower than the Inside temperature reading. Also check the circuit breaker and reset if necessary. Make sure that the furnace door is closed securely. If “wait” is in the screen or “cool on” is flashing – wait 5 minutes for the system to safely respond. The thermostat will indicate it is asking for the cooling to turn on when "cool on" or a "snowflake" in the display. If this message is in the display, the thermostat is asking for the heat to be on and there is a likely a problem outside of the thermostat preventing the cooling from running.
There are several items you can check.
  • First check that the thermostat is set to the Heat position. Make sure the temperature is set higher than the Inside temperature reading.
  • Also check the circuit breaker and reset if necessary.
  • Make sure that the furnace door is closed securely.
  • If “wait” is in the screen or “heat on” is flashing – wait 5 minutes for the system to safely respond.
  • The thermostat will indicate it is asking for the heat to turn on when "heat on" or a "flame" in the display. If this message is in the display, the thermostat is asking for the heat to be on and there is a likely a problem outside of the thermostat preventing the heat from running.

For more information on the Honeywell heating and cooling systems, please click here to see a list of instructional videos.

If we weren't able to answer your question please visit Help & Support

USER MANUALS & GUIDES

Download PDF
Prestige IAQ Installation Manual
Model: THX9421R5021WW
English
Download PDF
Prestige IAQ Installation Manual
Model: THX9421R5021WW
French,Spanish