Wi-Fi Smart Thermostat (RTH9580WF)

$199.00

Get the App:

Get it on Google Play
Features
FEATURES
Our Wi-Fi Smart Thermostat lets you manage your home’s comfort and energy use with your smartphone, tablet or computer from anywhere in your home or the world. You can also receive alerts like maintenance reminders.
Setup
SETUP
Set up is simple and easy. First, verify compatibility with your home heating and cooling system and remove your existing thermostat. Now you’re ready for the step-by-step instructions for installing the Wi-Fi Smart Thermostat.

Staying comfortable by staying connected

With its customizable color touchscreen, our Wi-Fi Smart Thermostat is easy on the eyes. You can change the color to match your mood, paint choice or favorite team. You can also connect the thermostat to your home Wi-Fi and control the thermostat from your computer, tablet or smartphone. You can be anywhere—upstairs, across town or on the other side of the world and manage the thermostat remotely for comfort and savings.

  • Control from anywhere
  • Simple setup
  • Customizable color touchscreen
  • Smart response temperature timing
  • Indoor humidity sensor
  • Advanced fan/control comfort
  • Auto alerts
  • Locking touchscreen
  • Works with the Total Comfort Control app
  • One-year warranty
  • DIY installation
Total Connect Comfort App
Remotely monitor/manage your home’s comfort and energy use anytime, anywhere from your smart device (phone, tablet)
Auto Alerts
Receive system alerts to Wi-Fi enabled devices like filter status or service required
Smart Response
Thermostat learns your heating/cooling cycles, and then optimizes to deliver the right temperature at the right time. This way, your set program runs right on schedule.
Specs
  • Model number: RTH9580WF
  • Color: Silver
  • Dimensions: 3-1/2 in. High X 4-1/2 in. Wide X 7/8 in. Deep
Energy Savings
Click here to discover just how much you can save by installing a Honeywell thermostat!

Wi-Fi-Smart-Thermostat-Media

WiFi Smart Thermostat (RTH9580)
Honeywell Wi-Fi smart thermostat overview

Compatible with systems

  • This thermostat is compatible with heating/cooling systems and heat pumps.
  • It is not compatible with electric baseboard heat (120/140V).


Now you're ready for the instructions for installing the Wi-Fi Smart Thermostat. Simply choose the installation instructions option you prefer:

TCC App

Search “Total Connect Comfort” in the App Store or Google Play. Download the app to your smartphone or tablet to learn how to control your thermostat from anywhere, anytime.

Video-Guided Installation

Watch a video that will help you install the Wi-Fi Smart Thermostat.

Manuals and User Guides

Download PDFs of manuals and guides in the resources section below, such as Quick Start and User Guides.

Wi-Fi-Smart-Thermostat-Setup

WiFi Smart Thermostat (RTH9580)
Install the Honeywell Wi-Fi smart thermostat with the help of this video.
WiFi Smart Thermostat (RTH9580)
Identify Your Heating-Cooling System Type | Training | Honeywell
WiFi Smart Thermostat with Voice Control (RTH9590WF)
Connect the Honeywell Wi-Fi smart thermostat to your Wi-Fi network with the help of this video.
WiFi Smart Thermostat with Voice Control (RTH9590WF)
Register the Honeywell Wi-Fi smart thermostat with the help of this video.

SUPPORT ARTICLES

Often, the thermostat will separate from the wallplate with moderate pressure. Other times, there might be small screws holding the device in place. If you are unable to pull it off, please refer to your thermostat manufacturer's website or manual for removal instructions. NOTE: Do not place your old thermostat in the trash if it contains mercury in a sealed tube. Contact the Thermostat Recycling Corporation at http://www.thermostat-recycle.org/ or 1-800-238-8192 for information on how and where to properly and safely dispose of your old thermostat.
An extra unused wire in the wall can be used as the C wire for your new thermostat. The extra wire will also need to be connected to the C (common) terminal at the heating and cooling system. This will provide power to your new thermostat. Please refer to the video section for more information.
In most cases, the only tools and materials required are a small flat edge screwdriver, #2 phillips screwdriver, your thermostat ID card (located in the box), and your home Wi-Fi Network password.
The thermostat will have a glass tube with a silver liquid inside of the tube. Mercury is typically found in older mechanical thermostats like the Honeywell Round T87 and rectangular T8090.
NOTE: Do not place your old thermostat in the trash if it contains mercury in a sealed tube. Contact the Thermostat Recycling Corporation at http://www.thermostat-recycle.org/ or 1-800-238-8192 for information on how and where to properly and safely dispose of your old thermostat.
The C wire originates from your heating/cooling system and provides 24 volt power to your Lyric. "C" stands for common and there is no universal color used to designate this type of wire. If you do not have a C wire, your Lyric will instead draw power from your heating and cooling systems to power its battery.
There is no code governing wire colors and thermostat connections. The thermostat should be wired by the letters found next to the wire screw terminal block. If you do not know the letter labels, then you can trace the wires back to the air handler/furnace or heat pump/ac unit. That will allow you to determine the function of each wire at the system and then allow you to attach it to the matching terminal on the thermostat.
If you do not have a wire connected to a C terminal or one that is labeled C on your old thermostat, there might be an extra wire that is pushed into the wall or wrapped around the wire bundle coming from the wall. Gently pull on the wire bundle to check whether there are any additional wires. If you do not have any additional wires, please refer to the Install Videos for alternative wiring.
Honeywell offers several resources to assist in the wiring of your new thermostat. These resources include: Installation videos, a User Guide and a Quick Start Guide. If you are still unsure if your new thermostat is wired correctly, please contact Honeywell Customer Care at 1-855-733-5465.
A COM terminal is often used as another name for the C terminal and issued to provide power to your thermostat. COM can also refer to a communication circuit and will not provide power to the thermostat. If you have both a C and COM terminal on your heating and cooling system the thermostat should be wired to the C terminal. Please refer to the Quick Start Guide for more information.
Check the back or bottom of the router or the operating manual for the password. If you are still unable to find the password contact the router manufacturer.

If we weren't able to answer your question please visit Help & Support

Rebates

Looking for even more savings?

Based on your location you are eligible for the following offers. If this is not your location, please search by ZIP / postal code:

Offer
Constellation
$200.00 Per Home
Get up to $200 towards your Honeywell thermostat when you enroll with Constellation for both your home's gas and electricity supply. $100 for electric, $100 for gas, or $200 for both. This offer expires 2/28/17. Only new residential customers are eligible when they enroll in a new contract not terminated within 90 days. Check rates at https://shop.constellation.com/HONB/ or call 1-855-860-5076. Use promocode: HONB.

We're sorry there currently are no rebates available in this ZIP / Postal code.